Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU364AWK, series F6? (may be shown as F06)

Issue:
What are the repair parts for the HU364AWK, series F6? (may be shown as F06)

Product Line:
The list of repair parts is needed for Safety Switch catalog number HU364AWK, series F6.

Environment:
Heavy Duty Safety Switch

Cause:
Applicable only to HU364AWK, Series F6

Resolution:
The repair parts for the HU364AWK, series F6 (F06) are as follows. No other parts are available.
-Complete Line/Load Base (all one piece) - 4056703950 - (requires one line base per switch - includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line/Load Base mounting screws - 40205-464-01 (requires 6 per line base)
-Arc Suppressor Assembly - 40566-775-50 (requires one per phase; obsolete, no longer available, replaced by ASKE603)
-Arc Suppressor mounting screw - 40205-145-01
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 21401-222-40 (per lug)
-Switch Mechanism - 40566-786-50 (also requires Interlock Shaft Gasket 40567-860-01)
-Switch Mechanism mounting screws- 22999-405-62 (requires 2)
-Handle Assembly - 40566-635-50 (requires handle gasket 40566-031-01)
-Lockplate - 40566-721-01
-Lockplate mounting screws - 22999-405-62 (requires 2)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings