Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are molded case switches horsepower or motor rated?
Issue:
Looking for motor rated molded case switches.

Product Line:
Molded Case Switch

Resolution:
They are not specifically HP rated. Switches are chosen based on the rating of the overcurrent protective device (CB or fuse). The switch must be protected by a circuit breaker or fuse of equal or lesser ampacity, and the short circuit availability of the circuit must not exceed the withstand rating of the switch.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings