Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can an unfused 600A HVL switch connecting to a Power Dry transformer have the height reduced to 69`` from the standard 90``? Can it be UL listed?
Issue:
Unfused 600A HVL switch connected to a Power Dry transformer with the height reduced to 69 inch

Product Line:
HVL Switchgear

Environment:
Products sold and used in North America

Cause:
Product Selection

Resolution:
Yes. It will required 3 days of engineering time to reduce the height. It can be UL listed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings