Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the interior of ANY Square D (QO or Homeline) Load Center, be changed in the field to increase the spaces (or circuits) / amperage if the enclosure (box) is the same?
Issue:
Can a load center interior be upgraded to increase the spaces, circuits, or amperage if the box is the same?

Product Line:
Load Centers

Resolution:
No. The labeling on the enclosure and interior will not match and this will violate the UL listing and the National Electrical Code (NEC). Box label and interior label must match per NEC 110-3B code for labeling.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings