Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How to order a standard ``MH`` NEMA 1 back box with blank endwalls in both top and bottom?
Issue:
Order a "MH" Nema 1 box with blank endwalls in both top and bottom.

Product Line:
Panelboard Box

Environment:
NQ, NF Panelboard

Resolution:
Add the suffix ``BE`` to the standard box catalog number.
Example; MH44BE, MH74BE

NOTE: The endwalls on special MH boxes deeper than 5.75`` or wider than 20`` are blank as standard.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings