Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference between an 8501XDO and 8501XUDO relay?
Issue:
What is the difference between an 8501XDO and 8501XUDO relay?

Product Line:
Relays and Timers

Environment:
All products

Cause:
Product Features

Resolution:
The XUDO is a DC relay designed for utility applications. It is capable of up to 12 poles (XDO is 8 poles max), and is suitable for use in ambient temperatures up to 145 deg F.


CTA-ID : 2016214

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings