Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can an ELM150HD, ELM250JD, GFM100FA, GFM150HD, or GFM250JD ground fault module be used on a two pole/single phase application?
Issue:
Can the add-on GFM or ELM accessories be used on a 2-pole application?

Product line:
Molded Case Circuit Breakers

Resolution:
Yes, it can be used on single phase loads but MUST be installed on a 3 pole breaker. The ELMs and GFMs are constructed in 3 pole width for use on 3 pole breakers only. The module will function properly using only 2 legs.

NOTE: For 2 pole or single phase application, use the outside poles.

See instruction bulletins below as reference:
48041-089-01 - Earth Leakage Modules
48041-088-01 - Ground Fault Modules

Schneider Electric USA
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings