Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are I-line interiors provided as standard with copper or aluminum bus?
Issue:
Bus bar material type on i-Line Interior

Product Line:
Panelboards

Environment:
I-Line

Cause:
Interior Content

Resolution:
As RTI (Ready to Install), the HCM and HCP construction interiors of 600A and less, are provided as standard with aluminum bus, with interiors of 800A and greater, being provided with copper bus.
The RTI HCJ interiors of 600A and less are provided as standard with aluminum bus, with some copper interiors available (Refer to Digest Section 9). 800A interiors are provided with copper bus.
The HCP-SU interiors, which are rated 800A, and HCR-U interiors, which are rated 1200A, are provided as standard with copper bussing.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings