Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are additional ground lugs available for the EZM main or EZM branch devices?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
EZ Metering

Resolution:
There are no available additional or alternate ground lugs for either the EZM main devices or the EZM branch devices. The EZM main devices will come standard with one ground lug from the factory that should be sufficient for the voltage system supply wires. The EZM branch devices will come with one ground lug per meter socket from the factory that should be sufficient for the downstream load from each meter.

NOTE: If an installer wants or needs to add additional ground lugs in a EZM main, that will be between the installer and the local code authority and/or utility company.

Schneider Electric USA

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings