Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are NEMA Type 12/3R safety switches provided with a hub opening in the top end wall?

Issue:
Product Features

Product Line:
Safety Switch

Resolution:
A hub opening is provided in the top end wall in NEMA 3R devices with an "RB" suffix. For all NEMA 3R devices with an "R" suffix instead of "RB", then a blank top end wall is provided. If conduit entry is required through the top end wall of the "R" suffix devices, a field cut hole is required. Watertight "H type" hubs should be ordered separately.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings