Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are single pole PowerPacT Q frames available?
Issue:
Single Pole Q-frame Circuit Breaker offer

Product Line:
Molded Case Circuit Breakers

Resolution:
There are no 1 pole PowerPacT Q frame breakers available.

NOTE: Consider using the PowerPacT B frame breakers for single pole applications.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings