Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a neutral bus bar be added to I-Line II busway sections that do not have them already?
Issue:
Ffield installable neutral to I-Line II busway

Product Line:
Busway

Environment:
I-Line busway

Resolution:
No. Neutral busbars are an integral part of the busway structure. They cannot be field installed later.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings