Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What class of fuse can be installed in a PQ3620G plug-in unit?
Issue:
Type of fuse that can be used in PQ3620G plug-in unit

Product Line:
I Line Busway

Environment:
Square D Busway

Resolution:
The bus plugs' insulators are not replaceable and an entire switch will need to be ordered.
It will accept a class H, K, and R fuse. It can also be converted in the field to accept a Class J fuse.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings