Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What size feeder conductor can be terminated in the MPZ5S40F?
Issue:
Wire range for MPZ Mini Power Zone products

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Feed conductor size determination

Resolution:

The 480V Primary Main Breaker FAL24015 has a lug kit AL50FA which has a wire range from #14 to 4 AWG in Copper or (1) 12–4 AWG in Aluminum


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings