Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What was a part number of a simple remote annunciator station used with the now obsolete line isolation monitor, IGD?
Issue:
Selection

Product Line:
Medical Panels

Environment:
NFPA99, NEC517.160

Cause:
For replacement purposes in the future, the identification of all components of a hospital isolated power system is a necessary initial step.

Resolution:
Two devices were often used. IA1C was furnished a red "hazard" alarm and "safe/silence" button mounted together in a single flush plate.
The IA1C assembly was installed in a separately furnished back box.  RA1WM offered similar functionality using digital technology, and similarly it fit into a single gang box.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings