Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do ANY of the EZM main devices come with the neutral bonded to the box from the factory?
Issue:
Product Design Features

Product Line:
EZM Metering Equipment

Resolution
No, the EZM metering equipment is "suitable for use as service equipment", but it does NOT have to be service equipment. The customer will have to bond the main neutral to the box, based on the application.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings