Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are factory installed compression lugs available for any of the general duty, heavy duty, or double throw safety switches?
Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Resolution:
Below are the options for Factory Installation of Compression lugs on Square D safety switches:
1) General Duty Safety Switches -
No Factory Installed Compression lugs. BUT some switches do allow for Field Installation of compression lugs, see each switch wiring diagram.

2) Heavy Duty Safety Switches - Factory Installed Compression Lugs are available ONLY on the 800A and 1200A Switches(See Current Digest for ordering information). Field installable Compression Lugs are available for ALL other amperages switches.

3) Double Throw Safety Switches - No Factory Installed Compression lugs. BUT some switches do allow for Field Installation of compression lugs, see each switch wiring diagram.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings