Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the available terminal covers for Multi-9 breakers?

Product Line:
Miniature Circuit Breakers

Resolution:
The following terminal covers are only for use on C60SP UL1077, C60H-DC, C60N, C60H, C60L, C60CTRL and RCCB-ID (AC,A-SI) type Multi 9s:

  • For a 1 pole, use 26975
  • For a 2 pole, use 26976
  • For a 3 pole, use (1) 26975 and (1) 26976
  • For a 4 pole, use (2) 26976

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings