Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are alternative lugs available to accept 3 - 600KCMIL wires on 800A MLO I-line panels?
Issue:
Terminal lug data on the 800a I-Line main lug panel

Product Line:
Panelboards

Environment:
I-line Panelboards

Resolution:
The only alternative lugs are copper mechanical lugs, or alluminum and copper compression lugs but the wire range does not change. These are only available as factory installed.
The standard lugs are (3) #3/0 - 500 kcmil per phase and neutral. If they require the 3 - 600KCMIL wires, they will need to change to a 1200A and change to copper mechanical lugs and select
the wire range. Again this can only be done as factory assembled and not in the field.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings