Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How is Medium voltage Metal enclosed switchgear derated for ambient temperatures above 40 degrees Centigrade, for example 45, 50 and 55 degrees Centigrade.
Issue:
Is there a derating for higher ambient tepmeratures associated with Metal enclosed Switchgear?

Product Line:
MV Metal Enclosed Switchgear

Environment:
Application

Cause:
Specifying

Resolution:
Switchgear is derated per IEEE Std C37.20.2-1993 per a formula in paragraph 7.4.1. Per these calculations the deratings for switches are below:

At 45 Deg C 600A derates to 490A / 1200A derates to 980A
At 50 Deg C 600A derates to 472A /  1200A derates to 944A
At 55 Deg C 600A derates to 454A /  1200A derates to 907A

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings