Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
If an HCRU panel interior is fed through a back fed main breaker does that leave the main lugs free for use as subfeed lugs?
Issue:
HCRU panel interior fed through a back fed main breaker. Main Lugs are free to be used as Sub-Feed Lugs

Product Line:
I-LINE Panelboards

Environment:
Products sold and used in North America

Cause:
Installation / Setup

Resolution:
No. The HCR-U interior is not available with main lugs mounted at the end of the bus stack. A branch mounted SL kit must be used.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings