Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is the QOB3150VH the largest breaker that can be mounted in an existing NQOD panel?
Issue:
Largest breaker that can be mounted in an existing NQ or NQOD panel

Product Line:
Panelboards.

Environment:
Products sold in the North America

Cause:
Product features.

Resolution:
Yes, because the QOB3150VH mounts in a branch location, requires 6 vertical pole spaces, and only 20A max breakers can be mounted across from it due to the rating of the branch connector.
Larger breakers must be installed as sub-feed breakers and are available in NQOD panels as factory assembled only. NQOD panelboards are no longer available, the interior retrofit or complete replacement to NQ is recommended.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings