Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the class R fuse rejection kits required to mount a class R fuse in a safety switch?
Issue:
Product features

Product Line:
Heavy Duty Safety Switches

Resolution:
No, the class R fuse rejection kits are ONLY for use as a safety feature to reject ALL other fuses that are not class R fuses. So the Class R fuse will mount in the switch without the rejection kit installed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings