Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the terminal lug wire range for EZM3600TB and EZM3600TBCU Series M04, main lugs terminal boxes and are there Alternate Lugs?
Issue:
Product Feature

Product Line:
EZM

Cause:
Clarifying lug wire range

Resolution:
There are two lugs per phase and neutral. Each lug will terminate (1) 1/0 AWG - 750 kcmil or (2) 1/0 AWG - 300 kcmil, AL or CU. Therefore, the device will accept (2) 1/0 AWG - 750 kcmil or (4) 1/0 AWG - 300 kcmil per phase and neutral.
See the CAD dwg for any Alternate lugs that can be used on these devices. Link to CAD dwg


Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings