Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the terminal lug wire size for EZM1600TB and EZM1600TBCU?
Issue:
Product Feature

Product Line:
Metering Equipment

Resolution:
The device will accept (2) 1/0 AWG - 750 kcmil or (4) 1/0 AWG - 300 kcmil Al/Cu per phase and neutral.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings