Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a single EZM branch device contain both three phase and single phase meter sockets?
Issue:
EZM Applications

Product Line:
EZM Metering

Resolution:
A single EZM branch device CANNOT contain both single phase and three phase meter sockets. Also, an EZM line-up that is single phase incoming and outgoing CANNOT contain three phase branch units. BUT an EZM line-up that is three phase incoming can contain both three phase outgoing and single phase outgoing meter sockets, but the appropriate EZM branch devices are required.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings