Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a QMJ364H, Series E2 (E02)?
Issue:
Design repair parts

Product Line:
QMB/QMJ Branch Switches

Resolution:
This QMJ device is only a single switch and it cannot be modified in the field to add an additional switch. Parts are listed per switch. Only the parts listed below are considered field replaceable:
-Arc Shield/Suppressor Assembly - 4052021450 (arc suppressor housing) and 4052017302 (arc shield) (1 each required)
-Load Base Assembly - 4052107050 (1 required, lugs and fuse connector assembly not included)
-Fuse connector assembly - 4052107650 (1 required per phase)
-Fuse mounting nuts - 2342702001 (3 required per fuse connector)
-Lug Assembly - 4025116251 (per lug)
-Lug mounting nut - 2342702200
-Load base mounting screw - 4020506501
-Handle Knob Kit - 4028343750

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings