Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a QMJ364T, Series E1 (E01)?
Issue:
Design repair parts

Product Line:
QMB/QMJ Branch Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:

The QMJ device is a twin switch, meaning it contains two switches in the one device. Parts are listed per switch. Only the parts listed below are considered field replaceable:
-Arc Shield/Suppressor Assembly (1 each required) - 4052021450 (Arc Suppressor Housing) and 4052017302 (Arc Shield)
-Load Base Assembly (1 required, does not include lugs, fuse connector assembly) - 4052107050
-Fuse connector assembly - 4052107650 (one required per phase)
-Fuse mounting nuts(3 per fuse connector) - 2342702001
-Lug Assembly (per lug) - 4025116251
-Lug mounting nut - 2342702200
-Load base mounting screw - 4020506501
-Handle Knob Kit - 4028343750


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings