Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is LR44199?
Issue:
Is LR44199 a disconnect switch part number?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
North American Products

Resolution:
This is the CSA listing number for ALL the Class 9422 disconnect switches.  It appears on a label stuck to the switch base or arc suppressor of the disconnect switch.  This number, unfortunately, cannot be used to identify the size or vintage of the disconnect switch.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings