Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the purpose of an anti-inversion clip used on a Class 320 meter socket?
Issue:
Product function

Product Line:
Metering

Resolution:
An anti-inversion clip, when installed in the top right side meter jaw of a lever bypass meter socket, prevents a Class 320 watt-hour meter from being installed upside down (inverted) and also rejects the use of a Class 100 or Class 200 watt-hour meter.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings