Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What effect does the installation of weathershields have on the minimum distance between a vertical (wall) surface and the Transformer ?
Issue:
Clearances of Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Transformer heat dissipation requires clearance from obstructions

Resolution:

The minimum clearance applies only to a Transformer without weathershields. Once that distance is established, you may add the weathershields without violating the clearance requirement.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings