Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the QO24L60NRNM, series G1 (or G01) load center?
Issue:
Design Repair Parts

Product Line:
QO Load centers

Resolution:
Only the parts listed below are considered field replaceable:
Complete Base Assembly - 4050714650 (lugs included) (This is the complete interior base assembly less the 2 ground bars)
Base assembly mounting screw - 2153310141 (1 required)
Ground bar assembly - 4023088750  (2 required)
Deadfront Trim - 4050714701 (DOES NOT INCLUDE ANY LABELS)
Deadfront trim mounting screw and washer - 2153310141 (screw; 2 required) and 2361502101 (washer; 2 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings