Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the door gasketing be obtained for Nema 3R/5/12 panelboards, I-Line HC-WP or NF MH-WP?
Issue:
Obtain the door gasketing for Nema 3R/5/12 panelboards, I-Line HC-WP or NF MH-WP?

Product Line:
Panelboards

Environment:
Products sold and used in North America

Cause:
Product Selection

Resolution:
Yes, order part number 80106-507-01 and this will have to be ordered per foot. (so customer will need to specify total feet required when ordering, and order must be placed on the Plant). The gasket is neoprene material.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings