Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How can an NF430L4C or NF430L4 interior with main breaker kit be installed into an MH68 box when the standard is an MH62?
Issue:
Interior to be mounted in non-standard taller box.

Product Line:
NF panelboard

Environment:
NA

Cause:
NA

Resolution:
The load end of the interior will need to be extended by 6``.  Use kit NF6RDE

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings