Issue:
Old product design features
Product Line:
UEZ Metering equipment
Resolution:
UEZ (Unitized EZ Stack) multi-metering equipment was available in versions that had maximum branch breaker ratings of either 100, 125, or 150 A.
None of the UEZ devices were available with 200 A branch breakers.
The following lists the type of devices and the replacement branch breakers:
Old product design features
Product Line:
UEZ Metering equipment
Resolution:
UEZ (Unitized EZ Stack) multi-metering equipment was available in versions that had maximum branch breaker ratings of either 100, 125, or 150 A.
None of the UEZ devices were available with 200 A branch breakers.
The following lists the type of devices and the replacement branch breakers:
- UEZ devices with 100 A maximum breakers accepted field installed, 2p, QO or Q1 breakers up to 100 A. For replacement breakers, use 2p QO breakers, 100 A maximum.
- UEZ devices with 125 A maximum breakers had factory installed, 2p, 125 A breakers, Q2M2125MB. For replacement, use QBP22125TM.
- UEZ devices with 150 A maximum breakers had factory installed 2p, 150 A breakers, Q2M2150MB. For replacement, use QBP22150TM.
Released for: Schneider Electric USA