Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: Is there a lug kit for 9T2F or other Epoxy Resin Encapsulated Transformers?

Issue:
Lugs for Epoxy Resin Encapsulated Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Epoxy Resin Encapsulated Transformers by SquareD by Schneider Electric

Cause:
Transformers over 15 KVA often have terminals that require lugs

Resolution:
The connections for Epoxy Resin Encapsulated Transformers are stranded copper wire. No lugs are required to connect them into the circuit.

The following video demonstrates wiring methods for Epoxy Resin Encapsulated Transformers:



Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings