Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an SC8L125S, Series M01?
Issue:
Need repair parts for the device.

Product Line:
CSED

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4056161350
Meter Cover Mounting Screws - (2) 4020513002K (contains 10 screws, but only 2 are required)
Utility Pullbox Cover - 4056172250 (includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover - 7329401401
Load Center Cover Hinges - (2) X2983
Load Center Cover Hinge Mounting Screws - (2) 2159414081
Dead Front Interior Trim - 4056167402
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws, but only 1 is required)
Load Center Interior - 4056164050
Load Center Interior Mounting Screw - (6) 2153217161
Meter Base Assembly - 4056210850 (includes meter base with the left, load side meter jaw, blade guide, and L-shaped connector assembled to the meter base)
Meter Jaw - (3) 7329794850
Meter Jaw Mounting Bolt - (3) 2271020242
Meter Jaw Mounting Keps Nut - (3) 2342702001
Meter Jaw Blade Guide - (3) 4052761901
Meter Sealing Ring - 2920910001
Line Side Phase Lugs - (2) 4025102451
Line Side Phase Lugs Mounting Bolt - (2) 2271020242
Line Side Phase Lugs Mounting Keps Nut - (2) 2342702001
Closing Plate - (2) ACP
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings