Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the SC12L200S, Series M01?
Issue:
Design Repair Parts

Product Line:
Combination Service Entrance Devices

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4056171950
Meter Cover Mounting Screw - 4020513002K (contains 10 screws; only 2 required)
Utility Pullbox Cover - 4056194450 (includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - 4056194250 (includes hinges and latch)
Load Center Cover Mounting Screws - (2) 2142217101
Dead Front Interior Trim - 4056192501
Dead Front Interior Trim Mounting Screw - 4020513002K (contains 10 screws; only 2 required)
Load Center Interior - 4056184850
Load Center Interior Mounting Screw - (2) 4020510001 and (1) 4020510201
Load Center Line Bussing Insulating Shield - 4056171401
Load Center Line Bussing Insulating Shield Mounting Screw - 4020513002K (contains 10 screws; only 2 required)
Meter Base - 7329882750 (jaws not included)
Meter Base Mounting Screw - (2) 2142717200
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Keps Nut - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Meter Sealing Ring - 2920910001
Line Side Phase Lug - (2) 4025116051
Line Side Phase Lugs Mounting Keps Nut - (2) 2342702001
Closing Plate - ACP
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings