Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What was the AIR rating of an older QOB breaker with a green toggle?
Issue:
What was the AIC rating of a QOB breaker with a green toggle?

​Product Line:
Miniature Circuit Breakers

Environment:
QOB Breakers

Resolution:
In the early 1970s a green toggle indicated a higher AIR rating of 10 kA. The standard at the time was 5 kA. After 1975 the handle was changed to the standard black toggle.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings