Issue:
PS3620G and PQ3620G Plug-in Unit installation fitting into the same busway type.
Product Line:
Busway power distribution
Environment:
PS3620G and PQ3620G
Cause:
N/A
Resolution:
Yes. However, the PQ catalog number is for horizontal busway applications, the PS catalog number is for vertical busway applications.
PS3620G and PQ3620G Plug-in Unit installation fitting into the same busway type.
Product Line:
Busway power distribution
Environment:
PS3620G and PQ3620G
Cause:
N/A
Resolution:
Yes. However, the PQ catalog number is for horizontal busway applications, the PS catalog number is for vertical busway applications.
Released for: Schneider Electric USA