Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What filler plate can be used in the 200 and 225 A EZM branch devices that accept the Q2 and Q frame tenant circuit breakers?
Issue:
Selection

Product Line:
EZM

Resolution:
The EZM branch devices that have an ANGLED breaker opening will use the filler plate EZMPCP. The plate will mount from the back side and the screws from the front side.
The EZM branch devices that have a VERTICAL breaker opening will use quantity (2) QOFP filler plates.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings