Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a NEMA 4X, stainless steel safety switch available in 800 A or 1200 A?

Article available in these languages: Spanish

Issue:
Product Design features

Product Line:
Heavy Duty safety switches

Resolution:
No, the maximum amperage offered in NEMA 4X, stainless steel is 600 A.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings