Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the catalog number EZML331225 be field converted from one meter socket position to two meter socket positions?
Issue:
Product design

Product Line:
EZM Metering

Environment:
meter positions

Cause:
Application

Resolution:
No, the top meter socket position is Not convertible. The main bus connections that are required for the meter socket are not installed at the factory and cannot be field installed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings