Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for a 24 Vdc shunt trip for an SE or SED circuit breaker?
Issue:
Is there a 24Vdc shunt trip for the SE or SED circuit breaker?

Product Line:
Molded Case Circuit Breakers

Environment:
SE / SED Circuit Breaker Shunt Trip

Resolution:
S3ST024DC2 is the part number for this shunt trip.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings