Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are optional lugs available for the Class 9422 fusible and non-fusible disconnect switches which will accept more than one conductor?
Issue:
Can you land more than one wire on the Class 9422 disconnect switches?

Product line:
Disconnect Switches

Environment:
Class 9422 disconnect switches

Resolution:
No, suggest the use of distribution block(s).

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings