Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the QOM1 and QOM2 breakers suitable for 48 Vdc loads?
Issue:
QOM1 and QOM2 on DC Voltage

Product Line:
Molded Case Circuit Breaker

Resolution:
QOM1/QOM2 type circuit breakers have no DC ratings. They can only be used on 120/240 Vac single phase systems.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings