Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can power to the shunt trip coil be maintained on an EDB, EGB, or EJB breaker with a shunt trip?
Issue:
Does the shunt trip on EDB, EGB, and EJB breakers have coil clearing contacts to clear current after being energized?

Product line:
Molded case circuit breakers

Resolution:
Yes, the shunt trips on the E frames have internal coil clearing contacts.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings