Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What materials are needed for mounting a NQOD430L100CU in a MH32 box instead of the standard MH26 ?
Issue:
Additional parts required to mount interior into nonstandard box.

Product Line:
NQOD Panelboard

Environment:
NA

Cause:
Installation

Resolution:
(1) 80110-290-02 deadfront extension
(2) 80110-288-02 6`` rail extension
(4) 21590-17081 screws

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings