Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can 3-phase IN, 1-phase OUT EZM branches be used in the same line up with 3-phase IN, 3-phase OUT EZM branch devices? Do the single phase OUT devices have to be used in certain positions?
Issue:
Installation of EZM branch devices

Product Line:
EZM Metering

Resolution:
The 3 phase IN, 1 phase OUT EZM branch devices can be used with 3 phase IN, 3 phase OUT branch devices in the same line-up as long as the system is 3 phase incoming. These devices DO NOT have to be used in any certain positions within the line up.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings