Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement cover to go over the plug-in opening for standard, indoor (not IP54 rated, not "M feature") I-Line II plug-in busway?

Issue:
Door for Bus plug port

Product Line:
Busway

Environment:
I-Line and I-Line 2

Cause:
Replacement Parts

Resolution:

The door cannot be purchased separately. The customer will have to purchase the entire Plug-In Base Assembly, which will come with a new hinged door. The P/N for the Plug-In Base Assembly is 45204-728-50.  Colors of the base and door are subject to change...ie. some bases are red , some grey; some doors are black , some grey .      If the (2) attachment screws for the original plug-in base assembly cannot be reused, order qty (2) screws, P/N 21594-18200, to affix the new plug-in base assembly to the busway housing.


busway

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings